AXIS#.MOTOR.INERTIA

Description

This parameter is the motor inertia. It is used to calculate the default velocity loop tuning gains (AXIS#.VL.KP ).

Context

For more information see Motor.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

kgcm² for rotary motors

Range

0 to 200,000

Default Value

0

Data Type

Float
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
AXIS1.MOTOR.INERTIA

500bh

11h

Unsigned32

-

1000:1

Read/Write

No

AXIS2.MOTOR.INERTIA

510bh

11h

Unsigned32

-

1000:1

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.MOTOR.INERTIA

6206

183E

Unsigned32

Read Only

-

AXIS2.MOTOR.INERTIA

71742

1183

Unsigned32

Read Only

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.MOTOR.INERTIA

6206

Float

Read Only

-